A contactor can stand on its own as a power control device or as part of a starter. Contactors are used in applications ranging from a light switch to the most complex, automated industrial equipment. Contactors are used in electrical equipment that is frequently turned off and on (opening and closing the circuit), such as lights, heaters, and motors. The function of the contactor is always the same: to make and break all power supply lines running to a Load or, as defined by NEMA, to repeatedly establish and interrupt an electrical power circuit.
The first device used to stop and start electric motors was a simple Knife Blade Switch. This was a lever that would drop a strip of metal onto a Contact to make the electric circuit. In the late 1800s, "throwing the switch" meant that someone had to stand next to the knife blade switch and level it into the closed position. Engineers discovered that the contacts quickly wore out because humans could not open and close the switch fast enough to prevent arcing, which corroded the soft copper switches with pits, making them more susceptible to dirt and moisture. More importantly, as motors became larger, the currents to operate them also had to become larger, creating a serious safety concern. It was physically dangerous to handle the switch. Mechanical improvements were made, but with their dangerous operation and short contact life, knife blade switches remained at a design dead-end.
The manual controller was the next step up the evolutionary ladder, offering several important new features:
Double-break contacts open the circuit in two places simultaneously. Dividing the connection over two sets of contacts allows you to work with more current in a smaller space than available with a single-break contact. In addition, the mechanical linkage consistently opens and closes the circuit, sparing the metal from some of the arcing experienced under knife blade switches.
With a manual controller, the operator presses a button or moves a switch that is integral to the electrical equipment being run. In other words, the button or switch is physically attached to the controller itself and is not operated remotely. When an operator activates a manual controller, the Power Circuit engages, carrying the electricity to the load.
Engineers eventually made a breakthrough with the magnetic contactor. A magnetic contactor is operated electromechanically without manual intervention. This means that the contactor can be operated remotely, without the need for putting a person in a potentially dangerous location. Magnetic contactors use a small control current to open and close the circuit.
The materials used to construct contacts or contactors are generally dependent on the kind of environment in which they will be used. Common contact materials are fine silver, coin silver, silver cadmium oxide, and the noble metals. In addition to these materials, special contact finishes may be required for certain applications. For example, if a relay is to be used in a mildly corrosive atmosphere, contactors should have a chromate conversion coating.
Another popular type of contactor is a Definite Purpose Contactor, which is an electrically operated switching device specifically designed for the heating, ventilation, air conditioning, and refrigeration (HVAC) industry. They are controlled by automatic thermostat control or manual pushbutton interfaces.
Mechanically interlocked contactors, like the ones pictured above, are designed for reversing 2-speed, reduced-voltage, type starter applications.
A diagram of a magnetic contactor. The following components can be found in a contactor:
The E-Frame, when energized by the coil, becomes an electromagnet. The armature, a companion to the E-frame, is connected to a set of contacts. The armature is movable but is held by a spring. When the coil is energized, the movable contacts are pulled toward the stationary contacts because the armature is pulled toward the E-frame. Once the two sets of contacts meet, power can flow through the contactor to the load. When the coil is de-energized, the magnetic field is broken, and the spring forces the two sets of contacts apart. Contactors are used when no overload protection is necessary, and at lower levels of electrical current. They are also operated electromechanically and use a small control current to open and close the circuit.
Some major applications of contactors include lighting circuits, heaters, and transformers. Contactors are often used to provide central control of large lighting installations, such as an office building or retail building. To reduce power consumption in the contactor coils, latching contactors are used, which have two operating coils. One coil, momentarily energized, closes the power circuit contacts, which are then mechanically held closed; the second coil opens the contacts.
Magnetic starters include a contactor as an essential component, while also providing power-cutoff, under-voltage, and overload protection. Electromagnetic contactors are actuated by electromechanical means. They make and break power circuits to such loads as electric furnaces, lights, transformers, capacitors, heaters, and, when overload relays or inherent protectors are used, motors. Pushbuttons and selector switches, like the ones on a control panel, are used in hundreds of manufacturing industries. Each button and switch is connected to a contactor for use in making or breaking an electrical circuit remotely. They are used in applications such as elevators, pools, food processing, pumps/compressors, lighting, hoists and cranes, battery chargers, printing presses, vending machines, and agricultural processes.
The major customer concern is the life expectancy of a contactor. The more frequently the contacts are opened and closed, the shorter the life of the contactor. As contacts open and close, an electrical arc is created between them. The arcs produce additional heat, which, if continued, can damage the contact surfaces. The faster the contact closes, the sooner the arc is extinguished, and the longer the life expectancy of the contact. There is, however, an issue with modern contactors that have been designed to close so quickly and with such energy that the contacts slam against each other and rebound, causing a bouncing action. This bouncing action is referred to as Contact Bounce, and when the contact bounces away, a secondary arc is created. The contacts slam together again and again, each time the bouncing and arcing become less and less. In addition to closing the contacts as fast as possible, it is desirable for the contacts to bounce as little as possible to reduce secondary arcing and wear.