Skip to content

What Is a Terminal Block?

A terminal block (also known as connection terminals or screw terminals) is a modular, insulated section that fastens two or more wires together and consists of an insulating frame and a clamping component. Often associated with DIN rails in either IEC or NEMA rating, their adjustability allows wiring to be centralized and makes it easier to manage complicated control circuits. Today's control wiring solutions are gradually becoming more and more complex as equipment is constrained to smaller and smaller spaces, and industry calls for more responsiveness and higher amounts of automation. Within the control board, these modular components are snapped firmly into place on a mounting rail.

When modifications in the circuit must be carried out, terminal blocks can be easily added or removed from the rail without interfering with other wire terminations. In addition to minimizing the complexity of control wiring, the plastic frames of terminal blocks also protect against shorts and subsequently provide increased safety to installers and service crews.

Insulating Body

The insulating body houses the current-carrying elements. The body insulates the wire termination to reduce the heat produced when current traverses through the wires. It also supplies a base for the clamping system and other elements, including switches and fuses. The body of the terminal block has specially constructed holes for easy access to the clamping screws. The body also has a mounting foot that allows the terminal block to be clipped on and off the mounting rail without experiencing deterioration. The space-saving style of a typical modular block allows high-density circuits to fit in a standard control panel. A 5 mm wide block can deliver up to 60 terminations per linear foot. Standard 6 mm single-level blocks produce up to 50 terminations per linear foot; double-level blocks can manage up to 100 terminations per foot.

Mounting Block Construction

Mounting block bodies can be constructed from Polyamide 6.6, Melamine 150, or Ceramic.

  • Polyamide 6.6 is a sturdy thermoplastic material, manufactured to work under any atmosphere and remain elastic and fracture-proof from -40 degrees Celsius to 105 degrees Celsius. This substance offers high insulation, tracking resistance, and a high flammability score. The durability and ease of handling of this material make it the most frequently used.
  • Melamine 150 is a resin-based thermoset plastic with an organic filler. Despite the fact that it's a far more fragile material than Polyamide 6.6, Melamine 150 provides a high level of resistance to heat radiation. It is highly recommended for purposes where the continuous running temperature is anywhere between 110 degrees Celsius and 140 degrees Celsius.
  • Ceramic is an exceptionally rugged material that can be utilized in extremely high temperatures approaching 250 degrees Celsius. Ceramic blocks can also operate in industrial plants with excessive dust deposits and abnormally corrosive atmospheres.

Current Carrying Parts

The current carrying parts consist of a current bar and a clamping device. The current bar, at the core of the insulating body, is constructed from copper or brass. The clamping device fastens the wire in the terminal block and creates a dependable electric connection between the wire and the current carrying bar. The dimension of these current carrying parts varies in regard to the amperage/wire size and the construction of the block itself. Depending upon terminal block layout, wires can be clamped in position using screws, a combination of screws and pressure plates, wire cages, or spring clamps. A screw is the easiest method of connection: A screw is utilized to secure the wire against the current bar. With screws and a pressure plate, the wire is constrained with a metallic plate, which fastens the wire when the screw is secured. With a wire cage, when the screw is tightened, the cage pulls upward and squeezes the conductor against the current bar. The large contact area provides exceptional contact properties. Because the screw does not have immediate contact with the conductor, wire damage is prevented. Even thin stranded wire can be connected without the use of additional Ferrules or wire pins. Spring clamps require a tool to open. The clamp encloses the wire to provide dynamic clamping. This extra holding action endures vibration.

IEC vs. NEMA Classified Terminal Blocks

Terminal blocks are categorized as DIN (IEC) or NEMA, depending on characteristics, which include panel mounting method, standards and approvals, and design characteristics. DIN type rails are IEC terminal blocks, which originated in Europe. DIN describes the channel or rail that the terminal block is secured to. The design offers more terminations per linear foot, which satisfies industry demands to maximize the number of terminations in a control panel. IEC blocks are easier to attach, wire, and mark than NEMA-style blocks. Rails are offered in 15 mm, 32 mm, and 35 mm widths. DIN blocks are typically compatible between manufacturers because the rail is standard and can be fashioned to manage a wide assortment of applications.

Approximately 60 % of the terminal blocks used in the U.S. are DIN type. Most designers give preference to DIN type because it offers:

  1. Space saving, small compact designs, and more units per foot.

  2. A wide range of block types for design flexibility.

  3. A worldwide recognition.

NEMA terminal blocks, referred to as American-style, contain self-lifting pressure plates, binder head screws, or box lug connectors. They are more frequently used for heavy-duty operations. However, NEMA blocks consume more panel space and offer fewer terminations per linear foot. Also, rail sizes differ across manufacturers, limiting the user's choices.

NEMA terminal blocks are:

  1. Cost-effective for some applications.

  2. More options for high current applications.

  3. Open construction, which allows for easier wiring.

Selecting the Right Terminal Block

Choosing the correct terminal block is straightforward. Just follow the steps below:

  1. Determine current, voltage, and wire size (AWG) to be used for the individual wire runs in the control or power distribution application.

  2. Define any special space constraints imposed by the application

  3. Considering the first two steps, select the appropriate rated feed-through terminal types to satisfy the electrical and space requirements. Select block widths. Double to block level and wire size if necessary to meet space requirements.

  4. Determine how many blocks (number of Poles) are needed, whether any blocks need to be jumped, and how the jumper connections should be made (which place).

  5. Select special function block (ground, disconnect, fuse, indicating types, switch) based upon application requirements.

  6. At the end of each terminal block assembly, wherever a change in terminal block size occurs or when a side of a terminal block is not used, specify it as an end plate. Unused sides of terminal blocks must not be left uncovered and exposed.

  7. Determine where isolation partitions are needed to provide visual separation or to contain creepage within the terminal assembly. To ensure safety, isolation partitions separate blocks with different amperage ratings or voltages to prevent current/voltage jumping from one to another. Partitions also indicate to the maintenance crew or electricians that there may be a different voltage in each of the groupings of blocks.

  8. For rail-mounted blocks, select the type of rail mounting. Calculate the length required by totaling the individual widths (thicknesses) of the terminal blocks, end plates, isolation partitions, and end stops.

  9. Mark wire terminations using marking tags.

Terminal Block Video Overview

 

 

 Have Questions? We’re Here to Help!

Call 800-575-5562 today. Our solutions experts are ready to assist you.