What Is a Programmable Logic Controller?
What is a Programmable Logic Controller?
Programmable logic controllers or PLCs are solid-state devices designed to perform logical decision making for control applications in the industrial environment. They were immediately accepted in the automotive industry and are found in countless applications in many industries. PLCs perform functions that formerly required relays, solid-state electronics, or mini computers. They are a lightweight device that's rugged and operates without fans, air conditioning or electrical filtering.
Programmable Logic Controllers are simple to program. They use a relay ladder language that's very similar to magnetic relay circuitry. Engineers, technicians, and electricians can learn to program the Programmable Logic Controllers without extensive training or experience. There are numerous advantages in using Programmable Logic Controllers versus a relay or solid-state electronics. In a Programmable Logic Controller, changes can be accomplished quickly, and in most cases, without hardware modifications to the controller. Programmable Logic Controllers are reusable and indicator lights on the Programmable Logic Controller at major diagnostic points assist in troubleshooting. It's reliable, designed for the industrial environment and easy to maintain. Along with its cost savings, the Programmable Logic Controller is flexible and able to perform multiple functions.
Programmable Logic Controllers have three components. These components are a processor, power supply, and an input/output (I/O) section.

Processor
The processor, or the brain of the system, is a solid-state device designed to perform a wide variety of production, machine tool, and process-control functions. Conventional electromechanical devices, relays and their associated wiring formerly performed these functions. Processors provide these same functions, in a wider scope and variety of control functions, with minimal effort.
The processor operates on DC power (± 5V), that is supplied by the power supply. Internal DC power is also routed through the processor and operates a portion of the I/O and devices connected to the service port. Once the ladder-diagram program is entered into the processor, it remains until changed by the user with one of the programming devices. The program is unaltered through power failure or power off conditions.
Power Supply
Power supply converts the input source power into voltages required for internal circuitry. In some cases, it also provides an isolated VDC supply to power DC input circuits, switches and other indicators.
(I/O) Section
Electrical noise, such as spikes in the power lines or load kick-back would have serious impact on a PLCs internal circuits since its CPU operates at very low voltages levels. This is where the Input/Output (I/O) portion plays a critical role. The I/O, both inputs and outputs, protects the CPU from electrical noise. The I/O section is where status signals are filtered to remove noise, validate voltage levels, and CPU decisions are made and put into operation. Inputs provide their status to a storage area within the CPU and outputs are driven from similar stored status in the CPU.
Real world devices such as pushbuttons, limit switches and sensors are connected through the input modules in the PLC. These modules detect a change in the state of input signals and provide a stored image to input elements in ladder logic. The input elements simulate the actions of relay contacts within the PLC. In turn, output elements are "energized," which produces desired output signals to drive loads such as motor controllers, contactors, solenoids, and pilot lights, via the output modules in the I/O's. As a general rule, each instruction in ladder logic requires one word of memory. Each instruction is programmed so that series contacts are ANDed and parallel contacts are ORed.
PLCs are available with operating voltages from 12V to 240V AC or DC, and I/O's up to 512.