All industrial electronic devices require power sources or power supplies. A power supply is an electronic mechanism that changes AC line power to one or more individual DC outputs. This is accomplished via circuits that convert electrical input power, either AC or DC. Simply put, power supplies change AC line voltage and current into DC power in preparation for consumption by another device or machine.
These systems are complex and have specific requirements. The intensity and the type of current used to power these industrial electronic devices are important to consider when picking the correct power supplies to make sure that the energy going to the circuit in question is powered correctly and the right type (i.e., DC or AC).
Power supplies can be broken down into families: Linear, Switching, and Unregulated. Within those families are categories: AC adapters, AC battery chargers, DC battery chargers, benchtop power supply, DC/AC inverters, DC/DC converters, and frequency converters.
The voltage produced by power supplies that are not regulated will vary depending on the load and on variations in the AC supply voltage. A linear power supply is useful because it has linear regulators that protect both the circuit and the power supply from overcurrent. Adjustable linear power supplies are essential test equipment for the laboratory and service shop that requires precision. Linear power supplies are heavier than switching power supplies, but carry the same power rating. Popular devices that the linear power supply powers are:
With a lighter and smaller packaging than the linear power supply, the switching power supply offers the same power rating as the linear. Switching power supplies also come equipped with built-in safety technology, such as its own circuit breaker on board if it runs too strongly. This power supply converts the AC source to a high voltage, which in turn is used to produce a DC current and voltage. The high voltage allows a switching power supply to be more efficient and requires less AC current to produce equivalent DC current. Popular applications of the switching power supply are commonly found in consumer electronics.
Unregulated power supplies are designed for high current applications at a low cost, when full regulation is not a requirement. These rugged, highly reliable power supplies are ideal for powering applications such as:
AC Adapters & AC Battery Chargers - AC adapters & AC battery chargers are power supplies that are ideal for converting the 120 VAC into the desired voltage of the targeted electrical device. These adapters are also used to charge the battery in the device that is being plugged into.
DC Battery Chargers - A DC battery charger is a device used to take energy in the form of a DC current and put it into a secondary cell or rechargeable battery unit by forcing electricity through it. DC battery chargers are very quiet and power sensitive. They are very rugged and reliable as they do not overcharge.
Benchtop Power Supply - Benchtop power supplies are great for handling high amounts of current, as they are heavy-duty in their construction. Equipped with either an analog or digital display, the benchtop power supply also features multiple outputs and binding post terminals. The Benchtop Power Supply is ideal for engineers or techs who demand variety. These power supplies are ready to handle loads with adjustable voltage and current output with a built-in circuit-breaking mechanism.
DC/AC Inverters - "True Sine Wave" inverters are made purposely for powering computers and other electronics in mobile and off-grid locations. One standard AC receptacle provides for easy connection. Versions are available to operate from 24 V to 32 V battery systems.
DC/DC Converters - Either step up or step down the voltage for a given purpose or a set current regulation.
Frequency Converters - Controls the frequency of the output waveform.
Power supplies can be found in many different combinations of families and categories. When selecting a power supply, it is helpful to know the power requirements.
The most important questions to have answered are the following:
The power (wattage) of the power supply should then be calculated.
Next, determine the family of power supplies needed, and finally, determine the category of power supply that will best fit the needs of the application.