Industrial Control

Empowering Industry: Advanced Energy Awareness Automation Solutions for OEMs and MROs

Written by Galco | Aug 21, 2025

In the dynamic world of industrial electronics and automation, energy efficiency is emerging as a critical concern for both Original Equipment Manufacturers (OEMs) and Maintenance, Repair, and Operations (MRO) specialists.

OEMs and MROs are at the forefront of innovation, responsible for designing equipment that not only meets performance expectations but also aligns with sustainability goals and regulatory requirements. Energy awareness is a critical aspect of modern equipment design.

THE SIGNIFICANCE OF ENERGY AWARENESS

OEMs play a pivotal role in shaping industrial processes through their innovative equipment designs. Prioritizing energy efficiency not only benefits end-users but also aligns with sustainability goals and regulatory compliance.

MRO specialists are responsible for maintaining and optimizing the operational efficiency of industrial equipment. Automation technologies significantly enhance their ability to achieve energy awareness and efficiency.

BENEFITS OF ENERGY AWARENESS THROUGH AUTOMATION FOR OEMS AND MROS

The adoption of automation technologies for energy awareness brings significant benefits to both OEMs and MROs:

  • Competitive Edge: Offering energy-efficient equipment sets OEMs apart in the market and appeals to environmentally conscious customers.
  • Cost Savings: Energy-efficient designs reduce operational costs for end-users, enhancing the appeal of OEM products.
  • Sustainability Commitment: Creating energy-efficient equipment aligns with sustainability goals and regulatory requirements.
  • Reduced Downtime: Energy-aware systems are less prone to unexpected failures, reducing downtime and increasing equipment reliability.
  • Improved Productivity: Real-time data and automation capabilities streamline maintenance processes, improving overall productivity.
  • Energy Cost Reduction: MROs can identify and rectify energy inefficiencies, leading to substantial energy cost savings for their organizations.

ADVANCED ENERGY AWARENESS AUTOMATION SOLUTIONS

Utilizing advanced automation product technologies empowers OEMs and MROs to design energy-efficient equipment while enabling MROs to optimize energy usage in industrial operations.

The following automation product and system solutions are driving energy awareness and efficiency for OEMs and MROs alike.

VARIABLE FREQUENCY DRIVES (VFDS)

VFDs are a cornerstone of energy-efficient industrial and operations automation. They can be leveraged to create equipment with adjustable speed control, resulting in increased energy efficiency.

Incorporating VFDs into equipment design allows motor speeds to be adjusted according to actual workload, conserving energy during periods of low demand. VFDs offer soft start and stop capabilities, reducing wear and tear on equipment components and extending their operational life.

Offering energy-efficient equipment provides a competitive advantage in the market and appeals to environmentally conscious customers.

 

AC MOTORS

AC motors, in conjunction with VFDs, can be paired and customized to match specific equipment requirements, optimizing energy consumption. AC Motors designed for compatibility with VFDs allow OEMs and MROs to create energy-efficient systems from the ground up.

Integrating energy-efficient AC Motors into equipment designs showcases a commitment to eco-friendly manufacturing.

 

POWER SUPPLIES

Power suppliesare often overlooked but are crucial for ensuring the reliability and efficiency of automation systems. Choosing high-efficiency power supplies reduces energy losses during the conversion process, making the overall system more energy-efficient.

Compact and efficient power supplies help reduce equipment, application, and process footprint, saving valuable space in industrial settings.

Reliable power supplies also contribute to overall equipment performance and longevity.

 

PROGRAMMABLE LOGIC CONTROLLERS (PLCS)

PLCs serve as the central control hub for automation systems, allowing equipment to be efficiently monitored and managed. PLCs interface with energy meters and sensors, providing real-time data on energy consumption.

System operators and designers can program PLCs to sequence equipment and processes in an energy-efficient manner, ensuring that machines are active only when necessary. These devices are capable of detecting abnormalities in equipment performance that may indicate energy wastage, enabling timely corrective actions.

 

HUMAN MACHINE INTERFACES (HMIS)

HMIs provide an intuitive interface to monitor and control equipment and display energy consumption data through user-friendly graphics, making it easier for MROs to identify inefficiencies.

Customizable energy dashboards on HMIs allow users to track energy usage in real time, fostering awareness among the workforce. HMIs generate detailed energy reports, helping identify trends and areas for improvement in energy efficiency strategies.

 

SENSING EQUIPMENT

Advanced sensing equipment is a valuable asset to enhance energy awareness. Sensing equipment provides data on the performance of industrial processes, helping OEMs and MROs optimize systems for energy efficiency.

Sensors can identify potential equipment failures before they occur, reducing downtime and energy waste. Sensing equipment can trigger automatic adjustments in response to changing environmental conditions, further optimizing energy usage.

 

CONTACTORS

Contactors are essential electrical components used to control the flow of electricity to motors and equipment. By using contactors that match the load requirements precisely, OEMs and MROs can ensure that energy is only consumed when necessary, optimizing energy usage.

Some advanced contactors provide soft start and stop features, reducing mechanical stress on equipment and minimizing energy spikes during startup. Contactors can be integrated into automation systems, allowing for remote operation and control, thereby facilitating energy-efficient scheduling.

Specialty bidirectional DC contactors are also helping emerging electric mobility, EV, HEV, charging stations, battery storage, and photovoltaic industries relying on high voltage DC current. These contactors respond to the awareness of safety when switching and disconnecting high levels of power independently.

 

LINE REACTORS

Line reactors are often used in industrial settings to reduce harmonics, mitigate voltage spikes, and improve power factor. They also help minimize harmonic distortion, improving the quality of electrical power supplied to equipment. This ensures that energy is delivered efficiently.

By reducing voltage spikes and transients, line reactors contribute to stable power supply, preventing equipment damage and reducing energy waste. Line reactors help distribute power uniformly across equipment, enhancing energy management and reducing losses.

 

CIRCUIT BREAKERS

Circuit breakers are critical safety devices that protect electrical circuits from overcurrents and short circuits. They ensure that electrical circuits are protected against overloads, short circuits, and faults, preventing energy loss and equipment damage.

In case of a fault, circuit breakers provide rapid interruption of power, minimizing downtime and energy waste. Some modern circuit breakers offer monitoring and diagnostic capabilities, allowing MROs to identify and address issues related to energy consumption.

 

CONCLUSION

Energy awareness and efficiency are paramount for OEMs and MROs in the industrial sector..

By embracing these product technologies and fostering a culture of energy awareness, industries can reduce operational costs, enhance sustainability, and stay competitive. The journey to a more energy-efficient future has already begun, and it starts with harnessing the power of automation.

Any Questions? Contact Us!

Our experts are equipped to help you find the right part you need and get it to you quickly.

Call 800-575-5562 for additional assistance.