Industrial Control

ABB's Battery Energy Storage System: Powering the Future of Renewable Energy with Advanced DC and AC Solutions

Written by Galco | Aug 21, 2025

 As the global energy sector continues its rapid shift toward renewable sources, Battery Energy Storage Systems (BESS) are emerging as critical infrastructure for ensuring reliability and efficiency. The capacity to store and release energy on demand enables the integration of intermittent renewable sources like solar and wind into the grid, helping to stabilize power supply during periods of low generation.

According to forecasts, the BESS market is set to experience tremendous growth, with annual revenue expected to climb from $1.2 billion in 2020 to $4.3 billion by 2025. Much of this expansion is driven by advancements in high-voltage BESS for renewable energy and more efficient energy management technologies. ABB is at the forefront of this evolution, offering a comprehensive portfolio of energy storage components for both the DC and AC sides of BESS installations, specifically designed to enhance efficiency, safety, and overall performance. 

Understanding BESS 

At its core, a BESS captures excess energy generated from renewable sources like solar panels or wind turbines, storing it for use when energy demand exceeds supply. This ability to shift energy use across time is essential for smoothing out the intermittency of renewables, providing utilities and businesses with reliable power even when generation is low. 

Today, many utility-scale BESS are deployed in tandem with solar photovoltaic (PV) systems. Most utility-scale PV installations operate at 1500 VDC, and matching the BESS voltage to this standard is essential for maximizing system efficiency. By aligning battery voltage with the solar array's DC input, system designers can avoid the need for costly voltage conversion equipment, resulting in greater space efficiency and lower upfront investment. 

The Shift to Higher DC Voltages for Improved Efficiency  

Traditionally, BESS operated at lower voltages like 12 VDC or 48 VDC, common in lead-acid battery systems. However, the advent of lithium-ion technology and the need for higher power output have pushed BESS voltage levels to new heights—now reaching up to 1500 VDC. Higher DC voltages provide significant benefits, such as: 

  • Increased efficiency: Higher voltage systems require less current to deliver the same amount of power, reducing energy losses. 

  • Reduced equipment costs: Matching battery and inverter voltages eliminates the need for intermediate conversion, saving space and reducing the overall system footprint. 

  • Scalability: High-voltage systems are better suited to large-scale applications, allowing utilities and commercial operations to efficiently manage their energy storage needs. 

ABB supports this shift to higher voltages with a full suite of DC-side components rated up to 1500 VDC. These components, designed specifically for the needs of modern BESS installations, offer integrated protection features and ensure seamless operation. 

ABB's DC-Side Components for BESS 

For a BESS to operate efficiently and safely at high voltages, the right components must be in place on the DC side. ABB provides a range of high-performance components that address critical functions such as isolation, protection, and monitoring. Key components include: 

  1. DC Disconnect Switches: Used to isolate the battery system during maintenance or emergencies, ensuring safe operation and easy access. 

  2. DC Circuit Breakers: Protect the system from overcurrent or short-circuits, which can cause significant damage if not mitigated swiftly. 

  3. DC Contactors: These are essential for remotely switching battery banks on and off, providing flexibility in energy management and safety during system downtime or fault conditions. 

  4. DC Surge Protection Devices (SPDs): Protect the BESS from harmful voltage spikes or surges caused by lightning strikes or grid disturbances. 

  5. DC Insulation Monitors: Monitor the integrity of the system's insulation, providing pre-fault warnings that help prevent damage from earth leakage currents. 

  6. Current Monitoring Systems (CMS): Continuously track key operational parameters such as current and voltage levels, helping operators maintain power quality and optimize performance. 

ABB's AC-Side Components for BESS 

On the AC side, where stored energy is converted and delivered to the grid or load, ABB offers a robust line of protection and control devices. These components ensure the smooth transfer of power, protect against overcurrent, and help maintain overall system stability: 

  1. AC Circuit Breakers: These protect the AC side from overcurrent and short circuits, a critical function in preventing outages or damage to connected equipment. 

  2. AC Surge Protection Devices: Like their DC counterparts, these devices protect the system from voltage spikes or surges on the AC side, safeguarding sensitive equipment and preventing downtime. 

  3. Residual Current Devices (RCDs): Detect ground faults and protect against shock hazards or potential fires by isolating faulty circuits in real-time. 

  4. AC Contactors: Remotely control and switch the AC side of the system, facilitating load management and enhancing operational flexibility. 

Ensuring Safety and Efficiency with ABB's Advanced Solutions

As the complexity of BESS installations increases, so too does the need for advanced safety measures. ABB's portfolio of high-voltage components not only supports the efficient storage and retrieval of energy but also ensures the system remains protected from electrical faults, voltage spikes, and potential hazards. The combination of disconnect switches, breakers, surge protection, and monitoring devices forms a comprehensive protection scheme for modern energy storage systems. 

In addition to hardware, ABB's solutions offer digital connectivity for system monitoring and diagnostics, enabling predictive maintenance and reducing the risk of unexpected downtime. This level of smart automation helps reduce operating costs while enhancing overall system reliability.

ABB: Leading the Charge in BESS Innovation

With over a century of expertise in electrical engineering and energy management, ABB is a trusted leader in the development of next-generation energy storage systems. Their commitment to innovation ensures that system designers and operators have access to the latest high-voltage components, fully integrated with cutting-edge monitoring and control systems. 

As renewable energy continues to grow, BESS will be key to unlocking the full potential of solar and wind power. ABB's solutions are designed to meet the needs of this rapidly evolving market, providing both the efficiency and protection required to ensure long-term success. 

Conclusion 
BESS are pivotal to the future of renewable energy, enabling the reliable and efficient use of intermittent resources like solar and wind. As the industry moves toward higher DC voltages to match solar PV systems, BESS technology must evolve to meet new efficiency and safety demands. With ABB's extensive portfolio of high-voltage DC and AC components, system designers can create storage solutions that are not only energy-efficient but also resilient and safe. 

For OEMs, panel builders, and utility operators, choosing ABB's components means ensuring that every aspect of your Batter Energy Storage System is optimized for the future of clean energy. 

Have Questions? We're Here to Help! 
Call 800-575-5562 today.  
Our solutions experts are ready to assist you.